3/30/2012 6:25 PM | |
Posts: 2 Rating: (0) |
Is there a Drive out there that will allow me to run a 15hp motor and a 20hp motor off of one drive with both motors running at the same time? Thanks. |
3/30/2012 8:39 PM | |
Posts: 2 Rating: (0) |
The motors are different size will this not matter? Thanks, Joel |
4/2/2012 7:41 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, If the total power ratingdoes not exceed the limits of the drive no problem. http://support.automation.siemens.com/WW/view/en/14390055 For more about this isue. Regards, Marcjan |
Problem solved? |
|
Follow us on