(0)| 9/24/2012 1:38 PM | |
|
Joined: 1/4/2007 Last visit: 1/13/2026 Posts: 1198 Rating:
|
Hello JankoHrasko, I recommend you to use the Step7 example program for the Siwarex U 7MH4950-2AA01. You can find it on the internet: http://support.automation.siemens.com/WW/view/en/17831309/133100 Into that Step7 example program the FB45 is handling the communication between the PLC and the Siwarex U module. The FB45 is using internal the SFB communication (in the past it was the SFC communication). The sending of commands or to read/send data from/to the Siwarex U module is quite easy.
Siwarexi |
Follow us on