11/21/2018 3:10 PM | |
Joined: 10/30/2018 Last visit: 7/7/2022 Posts: 63 Rating:
|
hmm thats wierd. 6ES7 677-2DB40-0AA0 is written on the ET200SP module itself . anyhow in the online Diagnosis it shows CPU as 6ES7 672-5SC11-0YA0 , its also not available , CPU 1515SP PC is available though . still cant get the correct CPU in HW config. UPDATE got it working: 1. must select 6ES7 677 2DBX2-0XX0 ,the part is 6ES7 677-2DB42-0GB0 (6ES7 677-2DB40-0AA0 written on the module is only spare part, don't know why) 2. In Hardware konfiguration change the CPU to ist CPU1505sp F (6ES7 672-5SC11-0YA0) or as installed ( can see from online diaganostics) , delete the HMI part and Hardware Configuration works |
Last edited by: wayse at: 11/21/2018 4:00:31 PMLast edited by: wayse at: 11/21/2018 5:11:13 PM |
|
Follow us on