3/18/2021 1:27 PM | |
Joined: 8/3/2009 Last visit: 6/27/2024 Posts: 13163 Rating:
|
Hello The Example with QR Code out of the Toolbox LINK is only for showing the QR Code and its only an example, of course you can change or extend it. For priniitng use the PrintScreen function... Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/18/2021 2:27 PM | |
Joined: 10/17/2017 Last visit: 6/10/2024 Posts: 19 Rating:
|
Thanks for your answer. I know this tool and link, but my project is a little bir complicated, i have four models and four different qr code, also my report has so many texts, some logos and one qr code. I will give you an example and you can see in the attachment list. I have four models and four different type of reports.How can i do this in wincc runtime advanced. I have to generate a qr code and i have to use it in report section and then i will print it. |
Follow us on