(0)| 8/11/2020 11:10 AM | |
|
Posts: 56 Rating:
|
Comos has an installable help, and one way to get the help removed is to uninstall the help system. It can also be that the help itself wasn't installed but manipulated the entry point for the help system is here C:\Program Files (x86)\COMOS\1033\Current\Help\English\start.htm by default it links to this directory: file:///C:/Program%20Files%20(x86)/COMOS/1033/Current/Help/System/en-US/index.html# The start.htm does not exist in a plain Comos installation, it will be copied there when you set up the Comos help system same as the content below /help/system Or somebody has put an alternative start.htm into this subfolder or your Comos gets started with an alternative menu using the /MN: parameter. example: comos.exe /mn:abc.xml abc.xml will be looked up here: C:\Program Files (x86)\COMOS\1033\Current\config\menu\ and used as a menu file, and within that menu file someone could have put in an alternative help page. |
This contribution was helpful to
|
|
Follow us on