3/12/2025 11:31 AM | |
Joined: 11/27/2023 Last visit: 3/14/2025 Posts: 5 Rating:
|
Hi! Oddly enough there are no mistakes from s7 300 side and it can see that Master is online in network diagnosis. If i switch roles and CP 342 - 5 becomes Master then the error is gone but for my project i need S7 1500 as a Master. I've already checked all similar topics and found no solution for me.What could i check to find the reason of this mistake? Thanks in advance! |
3/12/2025 11:49 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, When S7-300 is master, everything is working fine? (So data is exchanged) When S7-1500 is master, you get error in Profibus slave (S7-300) Did you parameterize the Transfer data right? (On both sides?) Best regards, Wizard |
3/12/2025 2:02 PM | |
Joined: 11/27/2023 Last visit: 3/14/2025 Posts: 5 Rating:
|
Hello, Wizard! To clarify for data exchange of S7 1500 i use DPWR DAT and DPRD DAT blocks and on the S7 300 side i use DP_SEND and DP_RECV blocks. Parameters of transfer data are matched, transmission speed is 1.5 Mbps, consistency parameter is total length, for S7 1500 input addresses correspond to output addresses on the S7 300 side, the output addresses of the S7 1500 correspond to the input addresses of the S7 300. |
3/12/2025 2:11 PM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, Please give us some more information. How did you parameterize, please give some screenshots. Pictures give more information then words. Best regards, Wizard |
3/13/2025 7:34 AM | |
Joined: 11/27/2023 Last visit: 3/14/2025 Posts: 5 Rating:
|
Hello, Wizard! Sending you a screenshot of General settings of CP 342-5 (Slave) in Step 7. It looks like i can attach only one screenshot at a time, shame, i have more, it it possible to upload them all at once? Or do I need to attach them always for different messages? |
3/13/2025 7:35 AM | |
Joined: 11/27/2023 Last visit: 3/14/2025 Posts: 5 Rating:
|
Here are the setting for CP1542-5 (Master) |
Last edited by: Egineer1 at: 03/14/2025 05:50:38 |
|
3/13/2025 7:45 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hi, You can zip all screenshots. And attach the zip-file Best regards, Wizard |
3/13/2025 7:58 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, You are using TIA Portal and Step 7 v5.x. Have you seen this link: have a look at how to adjust properties of Profibus DP network. Best regards, Wizard |
3/14/2025 4:59 PM | |
Joined: 11/27/2023 Last visit: 3/14/2025 Posts: 5 Rating:
|
Hello, Wizard! Sorry for late replay, yes, i've read this article and it didn't help me to solve the issue. Instead of attaching screenshots i'd rather give you my projects which i used for testing, i think it would be more convenient to check for mistakes because i'm pretty sure every parameter is set right... Projects are made in Tia Portal V17 and Step 7 5.7. Is it possible for you to check it please? |
Follow us on