3/6/2025 10:08 AM | |
Joined: 4/25/2015 Last visit: 8/22/2025 Posts: 114 Rating:
|
Hello everybody, I manage to downgrade with prosave and the file CP_15_19_22_V2_V17_0.fwf It shows on the panel the same Firmware version as in the V19 project V17.00.00.00_42.01 but when I try to transfer I still got the alarm " download canceled due to transfer error 8020AB001A06FFF4!" According to what I can find on internet, the firmware is not the right version!!!! Any idea how to solve this Best regards Claude ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/06/2025 14:46:20New subject after splitting |
|
3/7/2025 1:43 PM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16442 Rating:
|
Hello claude_reckinger The Error Number indicates that there are some files missing for Transfer, this is not always the imagefile itself. Use the Image Tool: https://support.industry.siemens.com/cs/de/en/view/109825750 or if it does not work (but now with PIU V2 it should also work with the new login in Siemens Website), use the offline installation that is also explained in the FAQ above (Chapter 1.2) This way works with any version of TIA and with any Image Version you want to use, but always the same way as here described in the offline Installation bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on