1/11/2022 1:17 AM | |
Joined: 7/28/2021 Last visit: 9/23/2022 Posts: 7 Rating:
|
BBritten, you are welcome! In my example, I used string instead of number for ButtonTextSize because the input for SVG, which is based on CSS, text size can be many things ( examples include: 10px 20% 5em smaller etc.). https://developer.mozilla.org/en-US/docs/Web/CSS/font-size#values |
1/12/2022 5:22 AM | |
Joined: 11/4/2021 Last visit: 4/19/2024 Posts: 64 Rating:
|
Hi AD_777777, I've also been messing around with the render templates trying to adapt the inbuilt flat button to a dynamic svg. I have a few questions if you don't mind:
Also, I updated the example you gave to fix the corners getting clipped and supporting transparent colors. Attached if it helps anyone else. If I get the full flat button or anything else working I'll post it. AttachmentBasicButton_v1-0-2.txt (897 Downloads) |
Follow us on