5/6/2025 3:02 PM | |
Joined: 2/20/2025 Last visit: 5/22/2025 Posts: 3 Rating:
|
Hello all, For a standarization I am looking into the OpenBridge platform. Now I have created a standard framework with a menu structure and the top menu bar. In the OpenBridge platform it is possible to switch between 4 color scheme's. I want to implement this on the WinCC Unified platform. I want to start a discussion on how to properly embed this in the current framework. The following options I think are available:
Creating a standard style takes a lot of time for each element I want to use. My preference would be to create a global script that automatically changes the color of the elements on screen. Would there be anyone who already has done this or has some idea's on how to implement this? |
5/7/2025 11:00 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello AutoGen_4755254 this could help creating own styles for standards: https://support.industry.siemens.com/cs/ww/en/view/109824234 (if you already know then ignore it Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on