3/13/2023 7:15 AM | |
Joined: 5/29/2014 Last visit: 9/4/2025 Posts: 72 Rating:
|
TIA Portal version: v17 Update 5 I have configured an MTP1000 Unified panel to store a data log and an alarm log on an SD card. In Comfort panels, I could download this data using the Comfort panel's webpage browser interface (after configuring it with a user and password). Is there a similar way to remotely download log data from an SD card in Unified panels? The Unified webserver doesn't seem to have any interface to access files on the SD card. I thought I'd find the answer in this resource: Configuring Logging for SIMATIC WinCC Unified Systems But it seems to assume I already have the data downloaded to my computer... or worse, implies that the only way to access the data is to remove the SD card from the panel and plug it into my computer. The ability to download the data remotely would be very convenient in case I need to obtain the alarm log and I have a VPN connection to the machine. |
Last edited by: Jen_Moderator at: 03/13/2023 11:46:09Text formatting optimized. |
|
3/13/2023 1:06 PM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi Zivilin, You can connect a network drive to your Unified Comfort Panel. Once connected, you can use the File Browser to copy the log files to the network drive. Or you can create a button and write a script to move the files to the network drive. Kind regards |
This contribution was helpful to
3 thankful Users |
Follow us on