(0)| 7/17/2006 7:26 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Catalin, I think the CPU928 is the one thats communicate with the CP516. There will be in the OB20, OB21 and OB22 somewhere a SYNCHRON-block {FB125, with the PAFE on it, when there is not 0 then there is no synchronisation}. Thats the one that is making the connection between the CPU and the CP in first place. When thats not working then other functions won't work either. [:o] Further FB199 (when not renamed/numbered) EXT-.... will do all work between the CPU and the CP in cyclic program flow. See the handbook :Memory Module CP 516 with Standard Functions Blocks for further details. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 7/17/2006 8:04 PM | |
|
Posts: 3 Rating:
|
how about connecting /diagnosing cp516 from pg? any info? |
Follow us on