(0)| 1/6/2007 4:59 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, Have you read the handbook: IP 240 Counter/Positioning/ Position Decoder Modul ? [;)] Some hardware components are checked via a test routine following power-up. If a fault is detected, the IP 240 sets the red MF LED. You can read out the error message from the IP 240 by invoking a configuring FB. The FB enters the error codes in DW 8 to 10 of the specified data block. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on