8/6/2006 12:20 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="imran"]RecentlyI have purchased a usb/mpi adapter. I already have Simatic Manager V5.1 with service pack 1. NowI am unable to install usb/mpi adapter. Is this because of simatic manager version or any thing else. I have windows XP professional on my laptop. Hi Imran, First off all please update your STEP7 with SP6 Service Pack 6 for STEP 7 V5.1then you have that version up-to-date! On the internet PC Adapter USB Now Available is also the contents of the delivery and the Windows versions where itmust be tested with, Windows XP Professional is there also between. If it is not version V1.2 then please install the new firmware of the USB/MPI adapter first Driver and Firmware for PC Adapter USB 1.2 also in this update is the newest handbook of the USB/MPI adapter. So what i should do: 1. update STEP7; 2. install CD or download for V1.2 (do not connect the USB/MPI Adapter yet); 3. connect the USB/MPI adapter and go to the PG/PC-interface to see if the USB/MPI adapter is installed and make the right connection Good luck |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
4/2/2015 4:30 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
Follow us on