(1)| 8/4/2017 12:02 PM | |
|
Joined: 9/30/2016 Last visit: 11/19/2025 Posts: 952 Rating:
|
I really ought to remember this but I don't and I can't find the answer here either - so here goes: I want to reset a SR flip/flop when a binary signal changes status and I only want a pulse (not a steady signal) I have tried with a N_TRIG (see attached screenshots) and the #Testbit_1 does switch between TRUE and FALSE but I am not getting any change at Q. What is wrong and how do I make it work ? Is there a smarter what to do this ? Attachmenttrigger.pdf (282 Downloads) |
| 8/4/2017 1:14 PM | |
|
Joined: 9/30/2016 Last visit: 11/19/2025 Posts: 952 Rating:
|
Hi mopS04, Thanks to you and Sandeep Bakoliya for answering. I just tried that and it does not LOOK like it is working either (see screenshots again) - but I am starting to think I need something more in the logic to achieve the desired functionality. I would like to be able to toggle with the input ("Auto_IF".User.WinCC_STS."KE01 StBy Man Act") and get the output ("Auto_IF".User.WinCC_STS."KE01 StBy Act") to toggle even then the input ("Auto_IF".User.WinCC_STS."KE01 Load StBy Act") is activated. In English I want to be able to switch the system out of StandBy by toggling the manual Standby even when the load-activated StandBy is on. Maybe if I use a SEL (can I use a boolean for 0/1 signals ?) and use the N_TRIG to make it switch between "Auto_IF".User.WinCC_STS."KE01 Load StBy Act" and a steady zero (and the OUT value goes to the SET pin of the SR in parallel with "Auto_IF".User.WinCC_STS."KE01 StBy Man Act" Any suggestions ?
Attachmenttrigger 2.pdf (246 Downloads) |
Last edited by: xmnj at: 8/4/2017 1:14:50 PMLast edited by: xmnj at: 8/4/2017 1:48:20 PM |
|
Follow us on