7/13/2023 1:17 AM | |
Joined: 7/13/2023 Last visit: 8/10/2023 Posts: 1 Rating: (0) |
Hey everyone, Bringing this back up to see if it was ever remedied? I'm having a similar issue. My AO card feeding the TB maxes out far to early and will not surpass 0.0026 volts (out of 1V possible). To be more specific when we input max value the meter stops at roughly 2.6/100 possible. -Changed display meters, didn't work -Changed AO cards, didn't work -Changed the TB, didn't work -I know the wiring is correct because when I change channels on the TB from 2 to 1 the meter displays correctly at max value -Next idea is to change out the back plate, but from this post it seems like that may be a waste of time. Software for the card is very basic and doesn't have possible faults as we proved it to work on the previous job (software was copied over nothing changed). From the last post it seems like if the meter were to go past 1V at a given point it might have blown something in the card? Any ideas? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2023 09:55:02New subject after splitting |
|
Follow us on