12/21/2022 6:08 PM | |
Joined: 6/25/2021 Last visit: 12/21/2022 Posts: 1 Rating:
|
Hey folks, I am having a problem using PLCSIM v15.1. I keep getting an error 33:17090 which says "A connection between your PC/programming device and the PLC cannot be established." I do have PLCSIM.MPI.1 set up through the Control Panel. What am I doing wrong? I did see here in another forum that indicated I needed to install SP2 (I have V5.6+SP1 of Simantic Manager installed) and the software is registered, I work for Amazon. HELP! ------------------------------------------------------------------------------------------ |
Last edited by: rjefhuds at: 12/21/2022 18:10:25Last edited by: Jen_Moderator at: 12/22/2022 10:51:29New subject after splitting |
|
12/22/2022 10:54 AM | |
Joined: 5/12/2006 Last visit: 6/14/2024 Posts: 22263 Rating:
|
PLCSIM V15.1 is for PLC S7-1200/S7-1500 Step7 V5.x is for PLC S7-300 so they can not work togeter. Which PLC you use exactly? If it is a s7-300 in Step7V5.x youn need PLCSIM V5.x |
This contribution was helpful to
1 thankful Users |
Follow us on