4/15/2021 1:30 AM | |
Posts: 5 Rating: (0) |
Hi, I have started with a simple project to be familiar with data exchange between 2 CPU's, I configured the hardware, one CPU 315-2DP as master and one CPU 313C-2DP as a slave and configured the Input/output in the Configuration Tab of the DP interface Object Properties, I run the Simulation to check the project but the I/O that have been configured does not respond, is there any tips that could help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/16/2021 07:00:02New subject after splitting |
|
Follow us on