9/4/2021 1:38 PM | |
Joined: 11/20/2018 Last visit: 6/9/2022 Posts: 3 Rating: (0) |
Hi , I have a Scalance Switch X101-1 6GK5101-1BB00-2AA3 The power supply is OK but LED P1 and FO are down no flushs , i made an essay : I connect my laptop to the P1 port with an RJ45 Cable --> no conection Two leds are On : led power L and led TL there is a button SET but i don't khnow how is works and if i need same config or paramtres I think there is no config needs to scalance X101 . I made a power On/OFF but i get always the same result no conections ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/06/2021 11:18:23New subject after splitting |
|
Follow us on