10/5/2021 1:24 PM | |
Posts: 257 Rating:
|
Since the IE/PB LINK PN IO converter is visually integrated into the SIMATIC ET 200SP series, it is sometimes necessary to supply the converter with power via the backplane bus of the ET 200SP. Although the converter has the housing technology of the ET200 SP, it is still an independent device and must be supplied via the connection X80 (see attached file). The device manual contains the relevant information on page 35 and from page 42 onwards. Note The procedure described in this article refers to the time when this article was written (status: October 2021). With Best Regards, SIMATIC International Technical Support Hub |
Last edited by: Jen_Moderator at: 10/06/2021 09:35:19Edited text for better reading. |
|
Follow us on