7/24/2018 7:09 PM | |
Posts: 50 Rating: (1) |
Dear all I've success build project Modbus RTU with S7 1200 and CM1241 in TIA v13 before. Now, I make a new project with new firmware and TIA v15 update 2. But it doesn't work. My configuration list here: - CPU1214C DC/DC/Rly 6ES7 214-1HG40-0XB0 v4.2 as Modbus RTU Master. - CM1241 RS485 6ES7 241-1CH32-0XB0 v2.2. - TIA v15 update 2. - Instruction MODBUS RTU v4.2 with Modbus_Comm_Load v3.1 and Modbus_Master v3.1. - Modbus RTU RS485 half duplex, 9600bps, None pairity, 1 stop bit After Modbus_Comm_Load done, CPU begin transmission data to Modbus Slave. But I've try to use some Modbus Slave (Power meter, Remote io) but can't see any data return. Modbus Master Status word value is 7000h or 7002h, only Tx blink. And finally, I use Modbus Slave Simulator software + USB2RS485 converter to test, COM port on my PC didn't receive any data request. I connect pin 3 + pin 8 on DB-9 port and also tried to swap. Any help Tks&Brs AttachmentProject1_20180724_2347.zip (73 Downloads) |
10/15/2021 10:39 AM | |
Joined: 11/15/2009 Last visit: 5/7/2023 Posts: 26 Rating: (2) |
Hi, Do you Resolve problem? Jaca |
10/15/2021 12:01 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi together, at first try to evaluate the error from the blocks right: How do you evaluate the status of system blocks in STEP 7 (TIA Portal)?TIA-help of the blocks tells you what the error-code means. hope this helps, regards, |
FCK WAR! |
|
Follow us on