10/29/2021 1:41 PM | |
Joined: 12/16/2014 Last visit: 9/26/2023 Posts: 4 Rating: (0) |
Thank you for this information. Of course, it doesn't help me, but at least I know the situation now. |
10/29/2021 2:08 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
Maybe you don't need the attachment, but this is an example for an easy program. In your case it is more work to handle different messages with the same keys depending on your program. With a free digital input you can create a setup switch as shown with I1. You also can use a menu with an up/down counter. The counter value then will activate the right message. But of course you need a lot of additional blocks. Regards, Scorp AttachmentTDE keys.zip (225 Downloads) |
Follow us on