12/16/2021 8:19 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi ep-ra, it seems that your TP-Link is not able to handle Profinet-Protocoll. So if you want to communicate via I-device you should change that device to one that also works on Layer 2. But you can also change to S7-communication or Open User Communiation. Application samples can be found here: How do you configure and program an S7 connection and the “PUT” and “GET” instructions for data transfer between two S7 CPUs?Basic Examples for Open User Communication (OUC)There are many other examples about these two ways of communication that may help you to get it work. hope this helps, regards, |
FCK WAR! |
|
Follow us on