2/15/2022 5:02 PM | |
Joined: 1/30/2022 Last visit: 5/21/2024 Posts: 1 Rating: (0) |
Hello gents i need help please i'm actually struggling unsuccessfully with reading signals on a 2AI cards AC5222 from ifm using AC1402 gateway with siemens PLC S7-1500 when give Node address 1 to my card it's ok i get reading on the first word (IW68) given in the Hardware config (4 words reserved by default from IW68.....75) but the problem comes when i change the node address to 2, 3, 4, etc...since i change the node address i can't get any reading although i tried to rewire my input word address from IW68, IW69, IW70, IW71 ......IW75 but when i tried to read signals from a 4DI/4DO ifm node AC5293 i can read the proxi switches signals for any node address i give to my card, in my exemple the addresses for all digitals signals start from IB4...19 and QB4...19, so if i give 9 as node address for my AC5293 i get all signals on IB8.4, IB4.5,IB8.6, IB8.7 i can change the node address for my digital card to whatever address i want and i am able to read the value but the issue come when i try to read the analog signals by changing the node address of AC5222 to any address i want Thanks for help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/16/2022 10:24:19New subject after splitting |
|
Follow us on