4/6/2022 12:32 PM | |
Joined: 9/4/2021 Last visit: 2/25/2024 Posts: 12 Rating: (0) |
hi my question is that i want to remote monitoring of s71200 remote location is approximately 35km from the actual site, kindly guide me may i used s7 1200 webserver and by using port forwarding method to remote monitoring of the data (i have a industrial vpn router welotec tk700) or some other method is also available in which more hardware is not required. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/07/2022 08:09:14New subject after splitting |
|
4/12/2022 9:24 AM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651) |
Hello khani456 Id depends on which Information you want to monitor of your S7-1200? For some simple information you can use the userdefined Webpages on the S71200 Webserver: https://support.industry.siemens.com/cs/de/en/view/68011496 If you need more functionality then you can use a HMI (Siemens HMIs have build in S71200/1500 communication driver through Profinet/ethernet). IF you have a system from third Party you could also use the OPC UA Server funkctionality of the new S71200 FW. Then your frontend needs only a OPC UA Client functionality. but of course for every solution you need a TCPIP connection. Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/10/2022 2:06 PM | |
Joined: 9/4/2021 Last visit: 2/25/2024 Posts: 12 Rating: (0) |
i just monitor sensor data digital /analog |
Follow us on