5/24/2023 10:03 AM | |
Joined: 9/11/2015 Last visit: 9/2/2024 Posts: 3 Rating: (0) |
Hello I am also trying to read data from a huwai inverter. but keep getting Error 80BB from MB_client Invalid value at ActiveEstablished parameter (identifier for the type of connection establishment, seeCONNECT parameter): modbus tcp is enabled on huwai inverter wich have ip 192.168.0.41. anyone have a suggestion what i am doing wrong. the Cyclic interrupt block is called every 3000ms or have a sample project that is working with huwai inverter ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2023 08:41:27New subject after splitting |
|
5/24/2023 10:31 AM | |
Joined: 9/11/2015 Last visit: 9/2/2024 Posts: 3 Rating: (0) |
Here is DB13 |
5/24/2023 10:42 AM | |
Joined: 9/11/2015 Last visit: 9/2/2024 Posts: 3 Rating: (0) |
hi Thanks No i am getting Error code 80B7 insted, error code is not listed in help file |
Follow us on