7/8/2023 4:14 PM | |
Joined: 9/24/2022 Last visit: 10/12/2023 Posts: 1 Rating: (0) |
dear sir please may i know about latching, how can i create the booster pump? latching by 1 duty and stand by , when the A pump cycle completed then motor should run B , this is working in every cut-off. for example: when pressure maintain by 1 duty A after cut-off motor B will run to maintain the pressure. i am facing to find the latching relay function in S7 1200 plc . thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/10/2023 11:08:23New subject after splitting |
|
7/10/2023 3:40 PM | |
Joined: 7/7/2010 Last visit: 11/8/2024 Posts: 15388 Rating: (2443)
|
-(S)- will SET a digital output until a RESET -(R)- is activated (or someone accidentally includes a -( )- for the same tag and messes everything up). Use F1-Help to find all the instructions available for your PLC. Or, expand the instruction pane and look through all the options.
|
science guy |
|
This contribution was helpful to1 thankful Users |
7/11/2023 6:59 PM | |
Joined: 6/20/2017 Last visit: 11/8/2024 Posts: 443 Rating: (40) |
There are a lot of possibilities: with SET operator over a internal boolean or output, but also SR, or RS for the same kind of tags. Attachment2023-07-11 20_54_24-C__Data_Sistemi_=1040_06872_dev_06872_06872_As01_1A1_06872_Plc01_1A1_SB_TiaPorta.png (322 Downloads) |
Gustavo Antonio Banchetti Brucatori. |
|
Follow us on