9/18/2023 3:14 PM | |
Joined: 11/2/2018 Last visit: 9/19/2023 Posts: 10 Rating: (0) |
Configured IP |
9/18/2023 4:29 PM | |
Joined: 1/21/2013 Last visit: 7/12/2024 Posts: 2973 Rating: (469)
|
Hi Flewrety, If you are using a S7-1200 or S7-1500 PLC, the "GetStationInfo" command will help you get the information you need. Kind regards |
This contribution was helpful to1 thankful Users |
9/18/2023 5:07 PM | |
Joined: 11/2/2018 Last visit: 9/19/2023 Posts: 10 Rating: (0) |
does it only work with online devices? I need to know the configured address even if the device is offline |
Follow us on