11/20/2023 12:01 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, These blocks belong to the CFC library and are included in the CFC software and are also available in non PCS7 applications. They differ from libraries like AP library, IL and other because those are created for PCS7 exclusively. Most of the blocks are not updated anymore since a long time (around year 2000) and can be used without any change in code. There are two exceptions: FB5: TIMER_P (Pulse generator) Last interface change: 12/03/1999, Last modified: 06/06/2019 PS: The AP library features block: TimerP that replaces this block, except for usage in SFC types, then it's still TIMER_P. FB16: PA_CPU (Monitoring of PO licenses) Last interface change: 12/23/2020, Last modified: 12/23/2020 Here you need to check if this can be downloaded in run since there is an interface change. This block is inserted automatically by the compile wizard and is generated in a system chart (@ chart). In the PUD manager under CFC library, you can find a description of all blocks. |
Last edited by: Oreca at: 11/21/2023 13:42:19If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
11/21/2023 4:43 AM | |
Joined: 4/28/2015 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
That makes sense. Thanks Oreca. |
Follow us on