11/27/2023 8:00 AM | |
Joined: 3/14/2008 Last visit: 11/14/2024 Posts: 2130 Rating: (953)
|
Hi, The modbus module is only released for PCS7 V9.1 SP2 or higher. You can check if a module is released via the link: Released Modules. If you really need it, you need to upgrade to V9.1 SP2. Please notice that the Windows version must be upgraded as well. Windows Server Standard 2016 is not supported anymore in PCS7 V9.1 or higher, only Server 2019. Maybe you can read through the following application example as well: Link It describes the communcation with the modbus module.
|
Last edited by: Oreca at: 11/27/2023 08:07:49Last edited by: Jen_Moderator at: 11/27/2023 11:13:50Links optimized. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
11/28/2023 8:46 AM | |
Joined: 3/13/2015 Last visit: 11/12/2024 Posts: 146 Rating: (40) |
Please take a look at the following link: https://support.industry.siemens.com/cs/ww/en/view/109822812 Valid for at least: PCS7 V9.0 to V9.1 SP2 Regards, |
12/3/2023 12:19 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Thank you very much but base on module datasheet that attached, in the Engineering part, siemens mentioned configurable with Step7 v17 or higher via GSD as of V5.6 HF4 that i not found any GSDML about that, so i think siemens datasheet is wrong. |
Last edited by: DPCS at: 12/03/2023 12:20:13 |
|
12/3/2023 12:25 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hi |
12/3/2023 4:39 PM | |
Joined: 6/23/2008 Last visit: 11/13/2024 Posts: 1168 Rating: (283)
|
Hello DPCS Molthoff's link is pointing to the documentation of the product "PCS 7 Library Modbus Advanced" which can be purchased as an addon to PCS7 and can be used from V9.0 on. You got that information already from me in my answer to your PM, but I would like to give the link to the product information for other readers here once more: https://support.industry.siemens.com/cs/de/de/view/109823110/en From V9.1 SP2 Oreca's link is very useful (also just for other readers). Even if I would recommend the addon library in your case (V9.0), because you also get the function blocks wich make the implementation much more comfortable (the function blocks mentioned in Oreca's link are only available from V9.1 SP2 on), I'm willing to help you to get the CM avilable in your version. Hopefully you are able to program the neccessary functions on your own... Also be aware that you won't have support of the driver wizard, but maybe you are able to program your own drivers supporting the driver wizard or waive the driver wizard support and just program a function by means of Step 7. I think your mistake is that you are looking for a single GSD for the CM. Instead look for the GSD of the ET200SP HA. I did that for you and you can use this link: https://support.industry.siemens.com/cs/de/de/view/109781191/en After installation of that GSD you have to put the profile in HW-config to "Standard". Then you will find the module under PROFINET IO -> I/O -> ET 200SP HA -> GSD -> Interface modules -> IM 156-6 PN HA V1.2 -> CM To be honest, I fear that you underestimate the efforts to program the neccessary functions on your own, but actually this is not the question... Would be nice from you if you reward my efforts to support you by a good rating... Best regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
12/4/2023 5:50 AM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hi mark1507 Thanks a lot for your explain and guidance but there are two problem: AttachmentAttachment.zip (346 Downloads) |
Follow us on