2/6/2024 2:57 PM | |
Joined: 7/19/2022 Last visit: 8/7/2024 Posts: 380 Rating: (62) |
Hello ThePapo, 1. To upgrade the STEP 7 Professional 2006 software license to STEP 7 Professional 2021, the license is the one you mention correctly (6ES7810-4CE12-0YE5). 2. Being STEP 7 Professional, the option packages are already included so you would not have to purchase a separate update for SCL or PLCSIM. With that you will update the licenses but not the software. You must install the software from: STEP 7 V5.7 SP1 / S7 GRAPH V5.7 SP1 / STEP 7 Professional 2021 SR1 Trial Download |
If this Information really helps, you could use the Rate function |
|
Follow us on