7/19/2024 4:38 AM | |
Posts: 1 Rating:
|
Hi I am trying to work out a solution where the S7-1500 is using TIM1531 module to communicate back to primary DNP3 Master over 4G network. I want to add some level of redundancy in the system by using a secondary 4G DNP3 Master so that the decision-making PLC gets the process variables from the field even when the primary 4G line is down. Is it possible to have multiple Masters for the TIM module? Are there any other modules that you can suggest achieving the solution apart from TIM1531? I can use another PLC (with TIA portal) if there is another solution. Could you please help? Thanks for your help. Warm regards, Roy |
Last edited by: AutoGen_7002000 at: 07/19/2024 04:45:04Last edited by: AutoGen_7002000 at: 07/19/2024 04:45:34 |
|
Follow us on