8/31/2024 12:48 PM | |
Joined: 8/31/2024 Last visit: 8/31/2024 Posts: 1 Rating:
|
I would like to run any Logo Soft Comfort on a Mac. I used to work with V7, so I do have the CD but no CD player anymore. I have a retired computer running OS10.15 Catalina and another one OS14 Somora. - On the first one I still have V7, but that does work anymore as v7 does not support Catalina. I tried to update via the update package did not manage to get it working. - I don't mind to pay for LSC8v, but I don't know how to get it running. I tried via de demo software with the expectation that I could pay for a full license. But also don't seem to get it started (I did updated my java software.) I am a bit of a lost here. Is there a download/pay button for v8, v8.1, ... that is compatible with an intel running OS14? thanks for the help, Benjamin ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/02/2024 08:38:49New subject after splitting |
|
Follow us on