3/30/2021 8:17 AM | |
Posts: 1 Rating: (0) |
i have same problem with ET200S this is my diagnostic buffer ------------------------------------------------------------------------------------------ |
Last edited by: IrvingVega at: 03/30/2021 08:18:22Last edited by: Jen_Moderator at: 03/30/2021 09:57:12New subject after splitting |
|
3/30/2021 2:49 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello IrvingVega, I have seen the firmware version of your ET 200S is V3.2.11 and so I recommend to update to firmware V3.2.17. Use in this case the link for the download. Firmware updates for IM151-8 PN/DP CPU (6ES7151-8AB01-0AB0) Compile also your complete project data with the both commands:
Also do a full reboot over voltage off and on again. With best regardsCicero |
9/14/2024 7:26 AM | |
Joined: 3/19/2019 Last visit: 9/14/2024 Posts: 102 Rating: (0) |
Hi IrvingVega, Did you got the solution for this?
|
"If you want the answer - ask the question" |
|
Follow us on