9/30/2024 7:32 AM | |
Joined: 8/6/2018 Last visit: 10/3/2024 Posts: 291 Rating: (40) |
Hello, I think it is not possible.You can see the information in control panel under panel information Thaks you |
9/30/2024 7:55 AM | |
Joined: 1/21/2013 Last visit: 10/4/2024 Posts: 3159 Rating: (490)
|
Hi, The @ServerMachineName system tag returns the hostname of the machine running the runtime. This hostname is built from the MAC address. So you can use it as a unique ID. Older image versions had the drawback that the hostname was restored when doing backup and restore, but in current versions the hostname is built from the MAC address each time the device is booted. Kind regards |
9/30/2024 8:40 AM | |
Joined: 9/26/2016 Last visit: 9/30/2024 Posts: 6 Rating: (0) |
Dear Expert, "Older image versions had the drawback that the hostname was restored when doing backup and restore", do you have specific image version information for reference? |
Last edited by: AutoGen_2103495 at: 09/30/2024 08:49:46 |
|
9/30/2024 9:29 AM | |
Joined: 1/21/2013 Last visit: 10/4/2024 Posts: 3159 Rating: (490)
|
Hi, As far as I know, the uniq hostname service was first introduced in V18.0.0.0. Kind regards |
Follow us on