10/4/2024 12:53 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, PLCSim does not allow you to have simulated hardware. You have driver connections (green lines) connect to the driver block which feed diagnostics and status signals from hardware, which do not work at the moment. You may have to use SimOn on the driver block to simulate the signals |
If I could help you, you can use the RATE button. Thank you. |
|
10/4/2024 11:15 PM | |
Joined: 3/1/2015 Last visit: 10/8/2024 Posts: 19 Rating: (0) |
Yes, I download every part of project |
Follow us on