1/20/2025 5:25 AM | |
Joined: 6/27/2024 Last visit: 8/16/2025 Posts: 3 Rating:
|
HI sir s7 200 plc i upload two diffent s7 200 cpu machine program after upload if i download program not download ,and i check compile some error show in my laptop , can you solve problem running program,how to show error (Compiling Program Block... MAIN (OB1) Network 2, row 1, col 3: ERROR 37: (operand 1) The memory addressing range is not valid for the instruction operand. Network 3, row 1, col 4: ERROR 37: (operand 1) The memory addressing range is not valid for the instruction operand. Network 264, row 1, col 3: ERROR 39: The call instruction does not have a corresponding subroutine. Network 265, row 1, col 3: ERROR 39: The call instruction does not have a corresponding subroutine. Network 266, row 1, col 3: ERROR 39: The call instruction does not have a corresponding subroutine. С�TIME (SBR0) �_1 (SBR1) HSC_INIT_0 (SBR2) �L (SBR3) �L (SBR4) SBR_5 (SBR5) SBR_6 (SBR6) INT_0 (INT0) INT_1 (INT1) Block Size = 0 (bytes), 5 errors) ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/20/2025 09:54:06New subject after splitting |
|
2/21/2025 10:50 AM | |
Joined: 2/21/2025 Last visit: 8/7/2025 Posts: 1 Rating:
|
Hello Sir Iam facing the same problem.Can any one help to solve this problem for me.
|
Follow us on