9/7/2006 1:51 PM | |
Joined: 9/1/2006 Last visit: 7/16/2024 Posts: 192 Rating:
|
Hi guys, It seems it is not possible to define a connection from the onboard Profinet-port to an "other station" using TCP. When i try to define the connection i get the error message: "No corresponding CP exists on the local station" If i adda seperate CP343-1 moduleI can easily define a connection in NETPRO to the other ethernet stations. How can i configure this connection (TCP or UDP) and then use AG_SEND/AG_RECEIVE to communicate between the onboard-PN-port and other CPU's with CP343-1 modules? Attachment319PN.zip (773 Downloads) |
9/7/2006 3:38 PM | |
Posts: 5822 Rating:
|
You are welcome. [;)] Best regards J_Bell |
9/8/2006 9:28 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Dear Remark, Since J_Bell already described the solution so maybe this is not necessary anymore but it could be helpfull to have a look at the following FAQ: How is an open TCP communication connection established between an S7-300 PN CPU and a CP343-1, and how is data exchanged? Best regards, INS |
Best regards, |
|
9/8/2006 11:01 AM | |
Joined: 9/1/2006 Last visit: 7/16/2024 Posts: 192 Rating:
|
Thanks INS, the samples in the doc will save me some time [:)] |
Follow us on