9/18/2006 12:01 PM | |
Posts: 4 Rating: (0) |
Hi: How can I Interconnected Automatically all the inputs of CH_MS Module? Bye. |
9/18/2006 1:24 PM | |
Posts: 4 Rating: (0) |
and where is the output Current( Active Motor Current) in the CH_MS block?. In my PCS7 doesn´t exist. In the manual A5E00345278-01 is present. Thanks. |
9/18/2006 2:17 PM | |
Posts: 3149 Rating: (171)
|
Hi the actual manual can be found here: http://support.automation.siemens.com/WW/view/en/21400491 some outputs of this block are not visible, so mark your block in cfc > properties > register connectors Normally the driver wizard will interconnect your inputs....if your hardware is supporting this inputs, so which hardware are you trying to run with this block??? nemo |
Follow us on