10/6/2006 4:25 PM | |
Posts: 3149 Rating: (171)
|
Hi, are you using AssetManangement, that´s a Maintenance station thought for.... http://support.automation.siemens.com/WW/view/en/16522013 did you proceed acc to this manual??? http://support.automation.siemens.com/WW/view/en/15229447 nemo |
10/18/2006 7:10 PM | |
Posts: 38 Rating: (2) |
Hi, If you want to test the display and the configuration data, you can start OS Simulation in the ES. Select the OS you want to simulate and Start OS Simulation. The OS configuration data is copied to a temporary folder and the OS Started based on this data. Please have a look at the following FAQ which may of interest and useful to you. http://support.automation.siemens.com/WW/view/en/23990630 Regards, PRK |
Follow us on