12/11/2010 7:42 AM | |
Posts: 111 Rating: (0) |
Hi dchartier, I have copied the prepard program existing in MB_ASCII of sample prject to my program. It contains OB1, OB100, FB7, FB8, FB10, FB21, FB23, DB40, DB41, DB42, DB43, DB50, DB70 and VAT1. I want youexplain me which one is send and receive blocks and which DB is its dedicatd DB. After putting slave address, the modbus function used, the start address and the length of data at the proper DB how could I access to these addresses and how to move to other slave.? How can I start sending data autmaticallybecause there is aM120.7 within the program ? and finally where were these read valued stored? Regards |
12/14/2010 10:39 AM | |
Posts: 111 Rating: (0) |
Dear all experts, Is there anyone to help me, I have really gotten cnfused by a great deal of documents. |
Follow us on