1/27/2011 4:47 PM | |
Posts: 6 Rating: (0) |
Hi, I have this setup at a customers site: S7-414 CPU with two CP443-1 (...1EX11-0XE0 fw.V2.3 and fw.V2.6) connected to one LAN (diferent IP, because of heavy traffic to some visualization) on the same LAN there is a S7-314 with a CP343-1 (...1EX30-0XE0 fw.V2.0) between these two CPs is an S7 connection (S7-300 is the active partner) which, unfotunately, terminates sometimes, irregulary. All connections come from the CP443-1 fw.V2.3 and there are also two more ISO-on-TCP, which IMO are not important, the second CP443 is only used for visu. In the CP343 there are 2 more connections to other PLCs which are working fine. At this moment the only way to restore the connection is to delete the S7 connection in NETpro, download connections and gateways without saving, and then reopen and download again with the appropriate S7 connection. thanks for any suggestions attached is the log from the two CP443-1 (important date 21.1.2011), there was nothing interresting in the CP343-1 log CP443-1 fw v2.3 buffer extract [code] ----------------------------------------------------------------------- 26.1.2011 14:14:23 Module type: CP 443-1 Module version: V 2.7.3 Hardware version: 4 Order number: 6GK7 443-1EX11-0XE0 S7 subnet ID of destination network: --- Address of dest. station network attachment: 172.16.2.130 Rack: 0 Slot: 5 ----------------------------------------------------------------------- 210 01/21/2011 11:08:27.132 AM OMS Event ID: 0xF9C1:0x0317 / 0x03E83107 Subsystem stopped after loading the existing SDB 1000 with assured consistency by the CPU containing the SDBs ; the existing SDB of type 0x3107 will be replaced since the time stamps are different. 211 01/21/2011 11:08:27.154 AM SEND/RECEIVE Event ID: 0xF9C1:0x261D / 0x00000001 The system connection to the CPU was terminated actively by the module. Internal info: 0x00000001 212 01/21/2011 11:08:27.159 AM SEND/RECEIVE Event ID: 0xF9C1:0x2615 / 0x00000000 System connection between module and CPU was closed 213 ! 01/21/2011 11:08:27.159 AM SEND/RECEIVE Event ID: 0xF9C1:0x261A / 0x0100E0E2 The module is terminating a connection actively. Connection number: 1 214 ! 01/21/2011 11:08:27.161 AM SEND/RECEIVE Event ID: 0xF9C1:0x261A / 0x0200E0E2 The module is terminating a connection actively. Connection number: 2 215 ! 01/21/2011 11:08:28.156 AM OMS Event ID: 0xF9C1:0x0326 / 0x03E83107 SDB 1000 is not listed in the still valid consistency assurance SDB or has an incorrect time stamp (SDB type 0x3107); the error will be corrected 216 01/21/2011 11:08:28.405 AM OMS Event ID: 0xF9C1:0x0317 / 0x03EB3002 Subsystem stopped after loading the existing SDB 1003 with assured consistency by the CPU containing the SDBs ; the existing SDB of type 0x3002 will be replaced since the time stamps are different. 217 01/21/2011 11:08:28.901 AM OMS Event ID: 0xF9C1:0x031C / 0x03F23118 The SDB 1010 loaded by the CPU containing the SDBs is the consistency assurance SDB (SDB type 0x3118) 218 01/21/2011 11:08:28.902 AM OMS Event ID: 0xF9C1:0x032C / 0x03F23118 Database now consistent after SDB 1010 was loaded by the CPU containing the SDBs (SDB type 0x3118) 219 01/21/2011 11:08:29.026 AM SEND/RECEIVE Event ID: 0xF9C1:0x2614 / 0x00000000 System connection between module and CPU was established 220 ! 01/21/2011 11:08:29.087 AM SEND/RECEIVE Event ID: 0xF9C1:0x260D / 0x0100E0E2 Connection 1 is not established. 221 ! 01/21/2011 11:08:29.109 AM SEND/RECEIVE Event ID: 0xF9C1:0x260D / 0x0200E0E2 Connection 2 is not established. 222 ! 01/21/2011 11:08:34.075 AM SEND/RECEIVE Event ID: 0xF9C1:0x260D / 0x0200E0E2 Connection 2 is not established. 223 01/21/2011 11:09:04.585 AM OMS Event ID: 0xF9C1:0x0317 / 0x03E93107 Subsystem stopped after loading the existing SDB 1001 with assured consistency by the CPU containing the SDBs ; the existing SDB of type 0x3107 will be replaced since the time stamps are different. 224 01/21/2011 11:09:04.610 AM SEND/RECEIVE Event ID: 0xF9C1:0x261D / 0x00000001 The system connection to the CPU was terminated actively by the module. Internal info: 0x00000001 225 01/21/2011 11:09:04.621 AM SEND/RECEIVE Event ID: 0xF9C1:0x2615 / 0x00000000 System connection between module and CPU was closed 226 ! 01/21/2011 11:09:04.622 AM SEND/RECEIVE Event ID: 0xF9C1:0x261A / 0x0100E0E2 The module is terminating a connection actively. Connection number: 1 227 ! 01/21/2011 11:09:04.625 AM SEND/RECEIVE Event ID: 0xF9C1:0x261A / 0x0200E0E2 The module is terminating a connection actively. Connection number: 2 228 ! 01/21/2011 11:09:05.559 AM OMS Event ID: 0xF9C1:0x0326 / 0x03E93107 SDB 1001 is not listed in the still valid consistency assurance SDB or has an incorrect time stamp (SDB type 0x3107); the error will be corrected 229 01/21/2011 11:09:05.895 AM OMS Event ID: 0xF9C1:0x0317 / 0x03EA3002 Subsystem stopped after loading the existing SDB 1002 with assured consistency by the CPU containing the SDBs ; the existing SDB of type 0x3002 will be replaced since the time stamps are different. 230 01/21/2011 11:09:06.327 AM OMS Event ID: 0xF9C1:0x031C / 0x03F03118 The SDB 1008 loaded by the CPU containing the SDBs is the consistency assurance SDB (SDB type 0x3118) 231 01/21/2011 11:09:06.328 AM OMS Event ID: 0xF9C1:0x032C / 0x03F03118 Database now consistent after SDB 1008 was loaded by the CPU containing the SDBs (SDB type 0x3118) 232 01/21/2011 11:09:06.522 AM SEND/RECEIVE Event ID: 0xF9C1:0x2614 / 0x00000000 System connection between module and CPU was established 233 ! 01/21/2011 11:09:06.564 AM SEND/RECEIVE Event ID: 0xF9C1:0x260D / 0x0100E0E2 Connection 1 is not established. 234 ! 01/21/2011 11:09:06.566 AM SEND/RECEIVE Event ID: 0xF9C1:0x260D / 0x0200E0E2 Connection 2 is not established. [/code] AttachmentdiagBuffer.zip (130 Downloads) |
Last edited by: JaWe at: 1/31/2011 12:54 PM |
|
Follow us on