1/28/2011 10:27 AM | |
Joined: 1/27/2011 Last visit: 3/16/2011 Posts: 1 Rating: (0) |
Hello, I need help configure a vpn between MD741-1 and a Juniper firewall. The idea is to connect up to 100 customers without using a scalance device. The WinCC servers and Database servers are behind the Juniper firewall. I have a test environment at the moment and the vpn tunnel is coming up. I have one laptop connected to the MD741-1 and another to the firewall. I cannot ping either laptop. I have doubled checked my firewall rules and routing on the Juniper and everthing looks ok. I have disabled firewall on XP laptops. I have also installed wireshark on the laptops. If I ping from a laptop connected to the MD741-1, traffic reaches the other laptop and sent back but the MD741-1 doesn't seem to accept it. I have also set firewall rules on the MD741-1 to accept any traffic. Any suggestions. Splitted from MD741-1. |
Last edited by: O_Moderator at: 1/28/2011 11:41 AMnew subject after splitting |
|
Follow us on