instead of the ISO Protocol you can also use the TCP Protocol, but be sure that the Port 102 is opened for the PG Functions
11/22/2006 1:01 PM | |
Posts: 5822 Rating:
|
Dear Richard, well here is a Link to a FAQ that shows a bit of the doing, instead of the ISO Protocol you can also use the TCP Protocol, but be sure that the Port 102 is opened for the PG Functions: |
Follow us on