12/7/2006 1:08 PM | |
Posts: 8 Rating: (0) |
Hello, I've faced a serious problem with the installation of PCS7 V6.1+SP1. The following softwares have been installed before: SQL Server 2000 Service Pack 3a for WinCC V6.0 and Microsoft ServicePacks & Tools for WinCC . The attached file is a copy of my computer screen. I've even removed all the softwares previously installed in my computer and tried to re-instal PSC7 many times but the error still occur at the level of WinCC installation !! and if i click on "ok" , it will be impossible to save a new HW config in SIMATIC manager!What can i do ? Thank you AttachmentCopie de PCS7_ERROR.zip (495 Downloads) |
Follow us on