12/23/2006 11:41 AM | |
Posts: 17 Rating: (0) |
You have to have MPI down load cable .The same cable which you use to Download the S7-300,400 plc program. thanks |
12/27/2006 8:53 AM | |
Joined: 4/24/2006 Last visit: 11/19/2024 Posts: 8770 Rating: (1171) |
Hello serkan_boz, The mentioned cable is correct. You'll have to put OP3 in Transfer mode serial. Another option is to download using MPI. In that case you'll have to put OP3 in transfer mode MPI. Here is a link to manual: http://support.automation.siemens.com/WW/view/en/1142799 Best regards, Wizard |
Follow us on