8/26/2011 1:37 PM | |
Posts: 96 Rating: (10) |
Hiadilmahsan, I think you are talking about standard PCS7 server and not the CAS. You can detach a file in the winnCC alarm logging and then copy the file from the Wincc Project folder to a CD/DVD or harddrive. When you are importing the file then copy the file back in the same folder and in the alarm loggin attach the file again. Hope this was helpful. regards, mk
|
8/26/2011 4:01 PM | |
Posts: 96 Rating: (10) |
adilmahsan, This has been answered before. Please follow the following link or see attachment below the link. /tf/WW/en/Posts/23273
Hope this was useful. Regards, mk |
This contribution was helpful to1 thankful Users |
Follow us on