1/24/2007 9:31 PM | |
Posts: 26 Rating: (0) |
Estimated friend: To use a PT 100 with SIEMENS LOGO(SIEMENS LOGO 12/24 RC/RCoand LOGO 24/24o or SIEMENS LGO PT 100MODUL)you must use an analog inputs (See the pages 39 and 40 of the manual of LOGO! to conexionate the input). Well the second thing into the software you must use the analog input block or if you use the digital input block the inputs will be consideredas a digital inputs and it is an error(See 4.1 Analog inputs, page116 of the manual). To calculate the range of analog values into the software(you must see 4.3.6 of the manual page 135). Well finally you must only analog blocks for the analog signals. The pages of the manual that I have reference are of the Spanish version of the manual LOGO! A5E00380837. Best Regards. I come from Spain. antonio@lageselectronica.es |
Follow us on