6/7/2006 7:46 PM | |
Posts: 3149 Rating:
|
Hi, I´ve found a quite interesting FAQ: http://support.automation.siemens.com/WW/view/en/19687561 nemo |
2/27/2012 7:15 AM | |
Posts: 6 Rating:
|
Hi Nemo, The Link u hav mentioned is Broken... Can u Giv the Live Link.. Regards, Vinu |
2/27/2012 7:28 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Unfortunately that FAQ is not available. It meant"
Instead of that you can use the SFC51 (Read system status) function to determine which LED's are ON or OFF or FLASHING. Why are no messages from the S7 diagnostics buffer display in WinCC flexible? Best regards, Hristo Mihalev |
Follow us on