5/1/2012 1:56 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, OPC for S7-1200 was released here: http://support.automation.siemens.com/WW/view/en/46605536 V7.1 is for Windows XP V8.x supports Win7 Its the same OPC Server for S7-300 CPUs You don't buy the OPC server iself, it is contained in the bundle "IE Sofnet S7" to be used with the integrated Etnernet interface of the PC. Softnet S7 IE exists in a Lean version: max 8 S7 connections. Or in a full version: max 64 connections. If you need more than 64 connections, you must use a communication processor like CP1613 or CP1623+ Hardnet IE-S7. |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on