11/16/2012 5:32 PM | |
Posts: 14 Rating: (0) |
Is it possible to make teleservice of five S7-1200 plc's with one CP1242-7? Or each must have individual CP1242-7? Thanks! |
11/16/2012 6:09 PM | |
Joined: 7/7/2010 Last visit: 11/19/2024 Posts: 15411 Rating: (2446)
|
You can connect up the 5 PLCs via profinet (network switch), and have one teleservice module connected to one PLC. I believe with the latest updates to FW & TIA Portal V11, you should be able to connect to the other plcs if they are all within the same portal project. You can verify this with a quick post to Support Request |
science guy |
|
This contribution was helpful to1 thankful Users |
11/17/2012 9:35 PM | |
Joined: 5/4/2009 Last visit: 5/28/2024 Posts: 914 Rating: (40) |
Dear Ganes 10, Thank you for your clarification, would you please provide us with the way for making one CP as a "gateway" for a number of networked CPUs. Warm regards. Tomy. |
Aim Higher |
|
11/18/2012 11:49 AM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello Tomy, If you mean CP 1242-7 here, then it is not possible; as a CP is used together with one CPU only. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
Follow us on